Technical FAQs

Ask a Question

Does Square D offer a replacement QO or Homeline load center Directory Label?

Design repair parts

Product Line:
QO Load Centers

Repair parts


Yes. Square D offers a Generic directory label for both QO and Homeline load centers, catalog number LSDL. The label is sold in multiples of 50 and measures 10 3/4`` in height by 2 3/4`` in width, and has 42 circuits on the label.

NOTE: Original factory directory labels cannot be sent out due to the UL manifest on them.

CTA-ID : 2033384
Was this helpful?
What can we do to improve the information ?