Technical FAQs

Ask a Question

Does the Multi 9 GFP protector have any on-board overload or overcurrent detection means ?

Issue:
Does the Multi 9 GFP protector have any on-board overload or overcurrent detection means ?

Product Line:
Multi 9

Environment:

Cause:


Resolution:
No. This device is purely a ground fault detector. A separate upstream thermal or thermal-mag breaker ( such as the Multi 9 C60) is recommended for overload and short circuit protection .


CTA-ID : 2034621
Was this helpful?
What can we do to improve the information ?