Technical FAQs

Ask a Question

What are the nine current settings on the Vigirex relay catalog number 56372 (56372TD), or RH99M?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
The settings are 30ma, 100ma, 300ma, 500ma, 1A, 3A, 5A, 10A, 30A.


CTA-ID : 2034703
Was this helpful?
What can we do to improve the information ?