Technical FAQs

Ask a Question

Is the wire set screw for a breaker catalog number QO2100 available?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment.

Resolution:
The wire binding screw is part number 48820-015-01 for QO2100 & QOU manufactured after January 1999 . The manufacture date can be identified by the date code on the breaker.

NOTE: If not in Q2C, contact Cedar Rapids Customer Service for availability.


CTA-ID : 2034700
Was this helpful?
What can we do to improve the information ?