Technical FAQs

Ask a Question

Can the ZB4BZ62 pad lock attachment be used on the ZB4 or ZB5 22mm selector switches?

Issue:
Can the ZB4BZ62 pad lock attachment be used on the  ZB4 or ZB5 22mm selector switches?
Product Line:
ZB4 and ZB5 22mm padlocks
Environment:
22mm push button and padlock attachments
Cause:
Locking out a selector switch is needed for an application, giving limited access.  
Resolution:
No, Schneider Electric does not offer a padlock for the 22mm selector switches.  Suggest customer transfer over to the 30mm line of operators, or change out the selector switch to a keyed selector switch.
 
Was this helpful?
What can we do to improve the information ?