Technical FAQs

Ask a Question

What is the torque requirement for the lugs on a 600A main lug and neutral I-line panel?


Issue:
Torque spec for panel

Product Line:
Panelboards

Environment:
I-Line

Cause:
Installation and maintenance

Resolution:
For 3/8`` allen screw it is 340 in-lbs. For 1/2`` it is 450 in-lbs.


CTA-ID : 2034180
Was this helpful?
What can we do to improve the information ?