Technical FAQs

Ask a Question

What is the maximum size of wire that can be used with a H60XFA?

Issue:
What wire size can the lugs in the H60XFA accomodate?

Product Line:
PTCCB - MCCBS, EARTH LEAK&SWITC

Environment:
Enclosed Switches

Cause:
Wire size range for this switch

Resolution:
Use a #6 AWG, 75 degree C, copper wire for 60 ampere rating.
The lugs on this switch will accomodate 12-2 (Al), or 14-2 (Cu). Table 3.34 pg 3-13 Digest 176.

H60XGA Switch
Cad drawing for this product can be found here.
A solid neutral assembly, 100SNA, is available for this product.



 

Was this helpful?
What can we do to improve the information ?