Technical FAQs

Ask a Question

LA7F902: The instruction sheet for a LR9F7375 says this mounting plate is mandatory.

Product Line:

Tesys F line Contactors and Accessories
This elevator bracket is only needed if the overload relay is mounted directly to the F-Line contactor. It is to provide additional support of the overload relay. If the relay is separately mounted no mounting plate is needed at all.

CTA-ID : 2035787
Was this helpful?
What can we do to improve the information ?