Technical FAQs

Ask a Question

What is the lug cover part number for a NAL361200, NA361200 breaker

Product Line:
Legacy Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
Part number is the same both ends of breaker, excluding I Line back fed NA361200 breaker which requires only (1) is 48131-023-01


CTA-ID : 2035832
Was this helpful?
What can we do to improve the information ?