Technical FAQs

Ask a Question

Will the 8501XL mechanical latch attachment fit 8 pole relays as well as 4 pole?

Issue:
Identifying mechanical latch attachment for 8 pole 8501 type X relay

Product Line:
NEMA combination starters

Environment:
Products sold and used in the United States

Cause:
8 pole latching relay is needed

Resolution:
Yes. The latch attachment can be used on 2 to 8 pole units, except the 8501XMO master relay units.


CTA-ID : 2035860
Was this helpful?
What can we do to improve the information ?