Technical FAQs

Ask a Question

Can an 8903PB type lighting contactor be controlled with a two wire control scheme ?

Issue:     
Can an 8903PB type lighting contactor be controlled with a two wire control scheme ? 

Product Line:
8903 type PB lighting contactors 

Environment:
Products sold and used in the United States

Cause:
Can an 8903PB type lighting contactor be controlled with a two wire control scheme ? 

Resolution:
Yes. Use an interposing relay just like the 8903 Type L , Form R6 option. The wiring diagrams are shown in the GIC help files. Form R6 is not an option on the 8903 PB since they are only offered as open style devices.


CTA-ID : 2036021
Was this helpful?
What can we do to improve the information ?