Technical FAQs

Ask a Question

What is the catalog number for the Electrical Interlock Kit used on the CH364, CH364RB, CH364AWK and CH364DS Series F05 Heavy Duty Safety Switches?

Issue:
Current design accessories

Product Line:
Heavy Duty Safety Switches

Environment:
accessories

Cause:
Application

Resolution:
The electrical interlock kits that can be used with these catalog and series numbers are as follows:
(1) For the CH364 Series F05 the part numbers are EIK1(1NO/1NC contacts) OR EIK2 (1NO/2NC contacts) or the EIK201EV(which is the Elevator Rated Electrical interlock for Canada ONLY)
(2) For the CH364RB Series F05 the part numbers are EIK1 or EIK2.
(3) For the CH364AWK Series F05 the part numbers are EIK1 or EIK2
(4) For the CH364DS Series F05 the part numbers are EIK1 or EIK2.



CTA-ID : 2035157
Was this helpful?
What can we do to improve the information ?