Technical FAQs

Ask a Question

What is the difference between an H3612RB and an H362RB disconnect?

Issue:
Product Features

Product Line:
HD SS

Cause:
Product Features

Resolution:
The H3612RB is a 60A enclosure with a 30A interior. The H362RB is a standard 60A safety switch in a standard 60A enclosure.


CTA-ID : 2035121
Was this helpful?
What can we do to improve the information ?