Technical FAQs

Ask a Question

What are the repair parts for the CH362DS, series F5? (may be shown as F05)

Issue:
Previous design repair parts

Product Line:
Heavy Duty Safety Switches

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The repair parts for the CH362DS, series F5 (F05) are as follows. No other parts are available.
Line Base Assembly - 4056614850 (arc suppressor not included)
Load Base Assembly - 4056614451
Line & Load Base mounting screw - 4020515101 (3 for line & 2 for load)
Arc Suppressor Assembly - 4056635550
Arc Suppressor mounting screw - 4020514501 (1 required)
Lug Assembly - CL0306F (includes 6 lugs)
Mechanism Assembly - 4056646950 (NOTE: Handle Coupling, Cover Interlock Defeat Coupling, and Lockplate Gaskets may also need replacing)
Handle Coupling - 4056699850
Cover Interlock Defeat Coupling - 4056699750
Handle Assembly - 4056779850 (also recommend replacing Lockplate Gaskets)
Lockplate - 4056681201 (also recommend replacing Lockplate Gaskets)
Lockplate Gasket - 4050322802 (2 required)
Lockplate mounting screw - 2194918121 (2 required)
Ground Lug - 4025101652 - (2 total required)
Ground Lug Mounting Screw - 4020513503
Fuse Pullers - FPK0610 (1 required for switch)



CTA-ID : 2034924
Was this helpful?
What can we do to improve the information ?