Technical FAQs

Ask a Question

Is a replacement control coil available for 8903PBW10V38?

The V38 voltage code was for a 120/208 volt coil but this is now obsolete and replaced by either a 120 volt coil or a 208 volt coil. The 120 volt replacement coil is 9998PBV02 and the 208 volt replacement coil is 9998PBV08. These are kits that include both a solenoid and a rectifier.

CTA-ID : 2035180
Was this helpful?
What can we do to improve the information ?