Technical FAQs

Ask a Question

What Class of fuse does the CH366, CH366R, CH366DS and CH366AWK safety switches accept?

Issue:
Product design feature

Product Line:
Canadian Heavy Duty Safety Switches

Cause:
Fuse type

Resolution:
These switches accept Class H or K fuses as standard. Options include Class R fuses (field install Class R Fuse Kit HRK4060) and Class J fuses (field install Class J Adaptor Kit H600J). With Class H or K fuses installed, the switches are CSA approved for use on systems with up to 10,000 RMS Symmetrical Amperes available fault current. With Class R or J fuses and the appropriate fuse kit installed, the switches are CSA approved for use on systems with up to 200,000 RMS Symmetrical Amperes available fault current.

NOTE: DO NOT USE RENEWABLE LINK FUSES IN SQUARE D SAFETY SWITCHES. The use of renewable link fuses may adversely affect user safety, impair reliability and will void the warranty.

CTA-ID : 2035554
Was this helpful?
What can we do to improve the information ?