Technical FAQs

Ask a Question

Are direction indicating contacts available for a U-Line LU2B*** starter ?

Yes , these contacts are standard and marked terminals 81 & 82 for direction 1 and 81 & 84 for direction 2 on the LU2MB0** reversing block on the bottom of the device.

Note that these contacts do not open when the contactor is de-energized. They report the current direction or last direction the motor was run.

CTA-ID : 2036911
Was this helpful?
What can we do to improve the information ?