Technical FAQs

Ask a Question

Is a door included with the CQO160L225GC or CQO160M200C, Series S04, Load Center?

Issue:
Product Features

Product Line:
QO Load Centers

Environment:
cover door

Cause:
application

Resolution:
A cover is provided, but due to the size of this load center, the cover does NOT include a door as standard. A separate door kit is available if required, catalog number QODK602.
NOTE: The door is a 'box top' type, that mounts to the face of the cover and ONLY goes over the deadfront area of the Main breaker and branch breaker and does NOT go over the complete cover.



CTA-ID : 2037010
Was this helpful?
What can we do to improve the information ?