Technical FAQs

Ask a Question

What is the replacement cover (or tirm) for the CQO160L225GC, Series S04?

Issue:
Design Repair parts

Product line:
QO Load centers

Environment;
Repair Parts

Cause:
Maintenance

Resolution:
The replacement trim(or cover) is part number QOC60UC. The cover does NOT contain a door, but there is a door KIT available catalog number QODK60-2.
NOTE: The door kit is a shoe box type door, that attaches to the face of the cover and ONLY goes over the deadfront area of the branch breakers and the main breaker. It does NOT go over the complete cover


CTA-ID : 2037009
Was this helpful?
What can we do to improve the information ?