Technical FAQs

Ask a Question

Is it recommended to connect Power Factor Capacitors on the load side of the overload relay?

No, it is our recommendation to connect Power Factor Correction Capacitors between the contactor and overload relay.

CTA-ID : 2037028
Was this helpful?
What can we do to improve the information ?