Technical FAQs

Ask a Question

Are the CR1F contactors mechanically held or electrically held?

Technically, neither. They have a special magnet circuit that allows them to be magnetically held. The end result is that they act as if they are mechanically held.

CTA-ID : 2036582
Was this helpful?
What can we do to improve the information ?