Technical FAQs

Ask a Question

What is the maximum size of the rod the float kit number A6 with float switch 9036DW31 will be supported?

Product Line:
 
9036 flow switch 

Resolution:
 
Switch will support 12.5` max of standard brass rod without a compensating spring.


CTA-ID : 2036250
Was this helpful?
What can we do to improve the information ?