Technical FAQs

Ask a Question

What is the part number for a Run Command Relay for use with the Altistart 48?

Use any ice cube relay. Selecte the coil voltage to match the customer`s control power. Typical load on the contacts is 25ma at 24vdc.


CTA-ID : 2036425
Was this helpful?
What can we do to improve the information ?