Technical FAQs

Ask a Question

What are the repair parts for a 82455R, Series A1 Double throw Safety Switch?

Issue:
Repair parts

Product Line:
Double Throw Safety Switch

Environment:
Repair parts

Cause:
Maintenance

Resolution:

The parts listed here are the only field replaceable parts.
Blade assembly - 40538-596-50 (4 used per switch)
Top switch base assembly - 40538-595-50 (4 used per switch)
Bottom switch base assembly - 40538-593-50 (4 used per switch)
Base mounting screws - 21427-18241 (2 used per base assembly)
Handle knob assembly - 40284-357-50
Lug assembly - 40251-136-51 ( 1 used per base assembly)
Keps nut for mounting lugs - 23427-02200 (1used per lug)



CTA-ID : 2036489
Was this helpful?
What can we do to improve the information ?