Technical FAQs

Ask a Question

What is the ground fault pickup tolerance range for the QO130EPD breaker?

Product Line:
Circuit Breakers
QO-EPD

Environment:
Electrical Distribution Equipment

Resolution:
The ground fault pickup range is 30mA +/- 4.5mA.  Therefore the tolerance range would be 25.5 mA to 34.5 mA.  


CTA-ID : 2036509
Was this helpful?
What can we do to improve the information ?