Technical FAQs

Ask a Question

What is the operating temperature range of the 8910DP and 8910DPA contactors?

It is 0 degree C to 40 degree C. While ARI conducts some testing at 65 degrees, this is to simulate extreme conditions and accelerate aging of the device

CTA-ID : 2036741
Was this helpful?
What can we do to improve the information ?