Technical FAQs

Ask a Question

What is the suffix ``RA`` in the catalog number PQ3610GRA mean?

Issue:
What does the "RA" suffix indicate on a PQ3610GRA 100A/3P busway plug in unit?

Product Line:
I-Line Busway and Accessories

Environment:
Busway plug in unit selection 

Cause:
Clarification of catalog number

Resolution:
The ``RA`` suffix means the plug-in unit will include a Class R fuse rejection kit (``R``) and copper compresson lugs (``A``)in lieu of the standard aluminum mechanical lugs.



CTA-ID : 2037459
Was this helpful?
What can we do to improve the information ?