Technical FAQs

Ask a Question

What is the part number for the contact cover on a LC1F185 contactor?

The part number is LA5F18550. The cover is also called the arc chamber as there are arc suppressors built into the cover.

CTA-ID : 2039003
Was this helpful?
What can we do to improve the information ?