Technical FAQs

Ask a Question

What is the difference between AL1200P24K and AL1200P25K?

Product Line:
PowerPact Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
The AL1200P24K may be used with I-Line mounted circuit breakers (and OFF end only of unit mounted breakers). This catalog number provides one lug per kit.
The AL1200P25K is used only for circuit breakers furnished with line and load lugs, and this catalog number provides three lugs per kit.
The AL1200P24K can be used on the Powerpact M frame whereas the AL1200P25K can not.


CTA-ID : 2037643
Was this helpful?
What can we do to improve the information ?