Technical FAQs

Ask a Question

What is the part number for the replacement Service Entrance Barrier for a CQO132M125C100, Series S04, and CQO132M125C125, Series S04 load centers?

Issue:
Design Repair parts

Product Line:
Canadian QO Load Centers

Environment:
repair parts

Cause:
Maintenance

Resolution:

The replacement service entrance barrier is part number 40559-522-01. The label attached to the barrier is 40270-516-01.

NOTE: The service entrance barrier CANNOT be used to convert a main lugs load center to a Service Entrance main breaker load center.


CTA-ID : 2037486
Was this helpful?
What can we do to improve the information ?