Technical FAQs

Ask a Question

What are the repair parts for the CHU361, series F5? (may be shown as F05)

The repair parts for the CHU361, series F5 (F05) are as follows. No other parts are available.

Line/Load Base Assembly -40566-426-50 (requires one per switch. Arc suppressor assembly not included)
Arc Suppressor Assembly - 40566-694-51 (requires one per switch)
Lug Assembly - 40251-016-52 (per lug)
Switch Mechanism - 40566-107-50
Handle Assembly - 4056684150K
Lockplate - 40566-376-01


CTA-ID : 2037575
Was this helpful?
What can we do to improve the information ?