Technical FAQs

Ask a Question

What is a Form Y742?

It is a Form for a factory installed alarm switch on an 8539 combination circuit breaker starter. It is installed inside the breaker and is only available on the FA KA LA MA style breakers


CTA-ID : 2037648
Was this helpful?
What can we do to improve the information ?