Technical FAQs

Ask a Question

What is the Terminal Lug Data for a CHU365AWK, Series E4 or E5 Heavy Duty safety switch?

Product feature

Product Line:
Canadian HD Switches

Confirming lug wire range

The lugs on this device will accept (1) #1 AWG - 600 kcmil or (2) #1 AWG - 300 kcmil copper or aluminum conductors per phase.

CTA-ID : 2037681
Was this helpful?
What can we do to improve the information ?