Technical FAQs

Ask a Question

Is the cover and dead front interior trim included with the QO312ML1, Series S04 Load Center?

Issue:
Product Features

Product Line:
Canadian QO Load centers

Cause:
Clarifying standard features 

Resolution:
A cover is not included with this load center. Order QOC16UC separately. The deadfront interior trim for a NEMA 1(Indoor) cover is NOT a separate part, the trim is an integral part of the cover.


CTA-ID : 2037758
Was this helpful?
What can we do to improve the information ?