Technical FAQs

Ask a Question

On a GV7RE80 starter there is a port under the clear plastic cover with 2 pin holes with + and - above it. What is the function of this port?

The port with the two pin holes is a test port for the plant to use only when they test the device. This is not for customer use.


CTA-ID : 2037873
Was this helpful?
What can we do to improve the information ?