Technical FAQs

Ask a Question

What is the wire size accepted by the 8903 Type L lighting contactors?<br /><br />

The power terminals will accept 1 (one) #16 to #10 AWG and the coil terminals will accept (2) #16 to #12 AWG.


CTA-ID : 2040807
Was this helpful?
What can we do to improve the information ?