Technical FAQs

Ask a Question

What is the temperature rating of the lugs on a JDL, JGL, JJL, JLL , JDA, JGA, JJA, JLA Circuit Breaker?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
The temperature rating is 75 degrees C.


CTA-ID : 2040794
Was this helpful?
What can we do to improve the information ?