Technical FAQs

Ask a Question

Is there a LED on the Motor Logic base or feature unit solid state overload relays?

On early units a flashing red LED on the Solid State overload relay was included in the upper right corner to indicate the overload was working. However, this indicator was removed in 2004.


CTA-ID : 2040817
Was this helpful?
What can we do to improve the information ?