Technical FAQs

Ask a Question

What does the suffix CA mean on an EDB breaker?


Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
Special Ambient Temperature: 50° (degree C (Not UL, CSA or NOM Certified)


CTA-ID : 2040873
Was this helpful?
What can we do to improve the information ?