Technical FAQs

Ask a Question

What coil voltages are available for the Class 8536 Type Starters?

Voltage Code V01 - 24 volt 60 hertz
Voltage Code V02 - 120 volt 60 hertz or 110 volt 50 hertz
Voltage Code V08 - 208 volt 60 hertz
Voltage Code V03 - 240 volt 60 hertz or 220 volt 50 hertz
Voltage Code V04 - 277 volt 60 hertz
Voltage Code V06 - 480 volt 60 hertz or 440 volt 50 hertz
Voltage Code V07 - 600 volt 60 hertz or 550 volt 50 hertz
Voltage Code V99 - Must specify voltage for 60/50 hertz, check before assuming any given voltage will be available




 
Was this helpful?
What can we do to improve the information ?