Technical FAQs

Ask a Question

If an older model QED switchboard has an I-Line branch section, can the newer R and J frame breakers be mounted in it, if space permits?

I-Line circuit breakers are backward compatible into existing I-Line switchboard sections as long as the section is the correct width for the breaker frame size being installed and there is adequate breaker mounting space in the interior.


 
Was this helpful?
What can we do to improve the information ?