Technical FAQs

Ask a Question

What is the difference between catalog number CQO124M125C100 and CQO124M100CD, load center?

Issue:
Product Features

Product Line:
Canadian QO Load Centers

Environment:
Product differences

Cause:
application

Resolution:
The CQO124M125C100 is only CSA approved and the CQO124M100CD is Dual rated, both CSA approved and UL Listed.


CTA-ID : 2039292
Was this helpful?
What can we do to improve the information ?