Technical FAQs

Ask a Question

What is the part number for the optional lug for (1) 600 kcmil per phase for the LC, LI, LE, LX,LXI breaker?

Product Line:
Legacy Circuit Breakers
LC, LI, LE, LX, LXI

Environment:
Electrical Distribution Equipment

Resolution:
It is AL600LI7. The wire range is for (1) 500-750 kcmil per phase.


 
Was this helpful?
What can we do to improve the information ?