Technical FAQs

Ask a Question

Do we have a 200 A din rail mountable breaker?

Issue:
Do we have a 200 A din rail mountable breaker?

Product Line:
PowerPact H and J frame molded case circuit breakers

Environment:
This applies to unit mounted breakers only it does not apply to I-Line breakers.

Cause:
Want to be able to mount breakers on DIN rail.

Resolution:

Yes, Powerpact H & J frame 3-pole breakers can be DIN rail mounted. Use kit # S29305.  
DIN rail mounting kit (requires 15 mm depth on a 35 mm DIN rail)
Fits 3 pole module breakers only. (Not available in 2 pole)

See instruction bulletin, 48940-239-01.

CTA-ID : 2042502

Was this helpful?
What can we do to improve the information ?