Technical FAQs

Ask a Question

Where are the neutral lugs located in a FP221R, 30 amp, fusible disconnect?

There is a ground bar in the FP221R, but there is no neutral bar. This fusible air conditioning disconnect is designed to be used in a 240V AC circuit with ground. A neutral lug is not necessary.


CTA-ID : 2042603
Was this helpful?
What can we do to improve the information ?