Technical FAQs

Ask a Question

What tenant breakers are used in the EZM, EZMR and EZMH, 125A maximum branch, 1-Phase 3-Wire, IN-OUT..branch units?

Issue:
Tenant breaker type

Product line:
EZM metering

Environment:
Tenant breaker

Cause:
Maximum ampere rating of tenant breakers

Resolution:

These branch units will accept 2-Pole ONLY Type QO, QO-VH and QOH circuit breakers up to 125A maximum.


CTA-ID : 2042727
Was this helpful?
What can we do to improve the information ?