Technical FAQs

Ask a Question

What is the voltage and AIC rating on the Multi 9, C45 breakers?

Issue:
What is the voltage and AIC rating on the Multi 9, C45 breakers

Product Line:
Circuit Breakers

Environment:
Applies to C45 circuit breakers only

Cause:
Ratings for the C45 circuit breakers

Resolution:
For C45 circuit breakers, the 1 pole breaker is rated 5 kA @ 240V, and the 2, 3, 4 pole is rated 5 kA @ 415 V.
Was this helpful?
What can we do to improve the information ?