Technical FAQs

Ask a Question

Is the CQO48M30DSGP or CQO48M60DSGP suitable for use with generators with a bonded neutral?

Issue:
Application

Product Line:
Canadian QO Load Center

Cause:
Application question

Resolution:
These panels are suitable for use with unbonded generators only since it does not switch the neurtal.

CTA-ID : 2041239
Was this helpful?
What can we do to improve the information ?