Technical FAQs

Ask a Question

Do we have lugs for the Powerpact MG and MJ breakers that will accept (3) 750 kcmil conductors?

Issue:
Do we have lugs for the Powerpact MG and MJ breakers that will accept (3) 750 kcmil conductors?

Product Line:
Powerpact M

Environment:
Lugs

Cause:

Resolution:
No.  The following lug only fits the Powerpact P frame breaker.  The AL1200P7KU lug for unit-mount breakers only will accept (3) 750 kcmil compacted aluminum conductors only.


CTA-ID : 2041673
Was this helpful?
What can we do to improve the information ?