Technical FAQs

Ask a Question

Does Square D offer the Enclosure(or bucket) ONLY for the QMB3400LA Series D2 Circuit Breaker Device?

Issue:
Previous Design Repair parts

Product Line:
QMB Circuit Breaker Device

Environment:
Repair parts

Cause:
Maintenance

Resolution:
No, the enclosure ONLY cannot be obtained for the QMB3400LA. The complete device, with the circuit breaker, must be obtained. 


CTA-ID : 2044577
Was this helpful?
What can we do to improve the information ?